FAQ: Imported CCES Example won't build; what is the procedure to import an example?

Document created by CraigG on Sep 18, 2012Last modified by CraigG on Aug 28, 2013
Version 2Show Document
  • View in full screen mode

Question

I’m trying to work with one of your examples but after importing it, it won’t build successfully. Is there something I’m doing wrong?

 

=================================

 

Answer

Your problem is probably due to importing the example via File->Import and having the ‘Copy Projects into Workspace’ option being checked.  Note, this option is checked by default.

 

As stated within our EZ-Kit manuals, CCES users are encouraged to use the example browser to find examples included with the EZ-KIT Lite Board Support Package.

 

We only support using examples:

 

  • Via the example browser
  • Import in place in the installation


To avoid this issue, you should navigate to your workspace and delete the example - the default location for the workspace is: C:\Documents and Settings\<User Name>\CrossCore Embedded Studio\. Once deleted, you should then use the Example Browser which is available via Help->Browse Examples from within the IDDE.

 

For detailed information regarding this feature please use the following path in CCES Help:

<Help>\CrossCore Embedded Studio 1.0.x\Integrated Development Environment\Navigating Within the IDE\Help System\Viewing Examples\Example Browser.

Attachments

    Outcomes