FAQ: Doesn’t an Add-in license have a grace period?

Document created by ColinJ on Sep 6, 2012Last modified by ColinJ on Aug 28, 2013
Version 2Show Document
  • View in full screen mode

Question:

 

I’ve just installed a CCES Add-in license using the option ‘Install a temporary license and then register it via website’. Once installed the Status of the license is displayed as ‘Full, Not Validated, Expired’. Doesn’t this license have a grace period?

 

-----------------------------

 

Answer:

 

Unlike a CCES license an Add-In license has no grace period and must be activated before you can use it. Note that it must also be activated to allow the installation of its Add-in component.

 

For further information refer to the CrossCore Software Licensing Guide.

Attachments

    Outcomes