Setting up the AD5755

Document created by GrainneM Employee on Sep 6, 2012
Version 1Show Document
  • View in full screen mode

Thsi Video clip shows how to setup and use the AD5755, Quad Channel, 16-Bit, Serial Input, 4 mA to 20 mA and Voltage Output DAC.

It will demonstrate, using the evaluation board, how to set the part into both Iout and Vout modes.

It will show the on-chip diagnostics and fault recovery.

Finally it will showcase the benefits of the on-chip  dc-to-dc boost converter optimized for minimum on chip power dissipation and the efficiencies associated with this on-chip dynamic power control.

Attachments

    Outcomes