Advantiv™ EDID Editor

Document created by GuenterL Employee on Apr 16, 2012Last modified by GuenterL Employee on May 12, 2017
Version 22Show Document
  • View in full screen mode

Advantiv™ EDID Editor Z version 0.91 beta

 

This program is released in beta a version designed to coexist with EEdit 0.41 and eventually replace version 0.41.  Added features are:

 

  • Handles block types, VESA, CEA, Video Timing Block (VTB), Display Information (DI), Digital Packet Video Link (DVPL) and Custom
  • Handles VESA versions 1.3 & 1.4
  • Handles CEA multiple short video descriptor blocks
  • Handles all CEA extended tag block types
  • Includes all VICs CEA-861-E, F, F extended
  • Import types: binary, Quantum Data XMLs
  • Export types: Binary, Quantum Data XMLs, code structure for direct program inclusion
  • Reports: HTML and text formats

 

Please download it, try it and break it.  Let me know of issues or features that need to be addressed

 

Advantiv™ EDID Editor version 0.41

 

This program was designed to be an integral part of AVES software however it is a full stand-alone EDID editor able to read, create and write the standard VESA block along with multiple CEA blocks.  It is compliant with CEA861E, EEDIDrAr1 and HDMI specification 1.4b.

 

Installation:

Run the included .msi file to install the program.  I recommend using the default location if AVES is intended to be loaded later.  The installer will add a shortcut to the desktop and insert a short cut to Program -> Analog Devices -> AVES

 

This program requires .NET Framework 4 Client Profile.  The installer will attempt to install it however if that fails then the Profile can be found at:

 

http://tinyurl.com/2vgnszt

 

This tool is provided AS-IS.

 

If bugs are found or potential improvements noted please post a comment so I can improve/fix the program and upgrade it for future users.

 

ChangeLog:

  • 0.15 - April 16, 2012
    • Original release
  • 0.20 - May 11, 2012
    • CEA Speaker Allocation was not being saved correctly.  Fixed
    • Expanded Vendor Specific, Video Capability and Colorimetry Data Block information and configuration display
    • Improved parameter entry.
  • 0.25 - June 28, 2012
      • Fixed data output error
      • Added direct EDID memory reads/writes via AVESServer and Aardvark USBI2C adapter
  • 0.30 - August 7, 2012
    • Fixed irritating bug.
  • 0.31 - September 5, 2012
    • Bug fix
  • 0.32 - October 16, 2012
    • Bug fixes, typo and display issue
  • 0.33 - November 13, 2012
    • Bug fixes
  • 0.34 - November 13, 2012
    • Fixed script saving problem
  • 0.35,36,37 - November 20
    • fixed XP crash issue and problem with VSDB
  • 0.40 - May 7, 2013
    • fixed VESA Color Characteristics saved values, previous values were not wrong, just fixed interpretation
    • fixed decimal point globalization problem on checks and saves. (good for US and Europe standards now)
  • 0.41 - June 12, 2013
    • fixed error associated with saving the data block monitor name, it added extra an 'linefeed', instead of a 'space'
    • Added splash screen, no effect on functionality, just click on it to go through it faster
  • 0.90 - February 7, 2015
    • Initial beta release
  • 0.91 - February 20, 2015
    • Added Astro Design format import and export feature.
  • 0.93 - April 30, 2015
    • Several bug fixes
  • 0.95 - February 21, 2017
    • Fixed HDMI_HF MAX TMDS Character Rate issue
    • Added text import and export
    • Added HDR static metadata extended block
  • 0.96 - February 27, 2017
    • Fixed DTD VESA DTD block, saving incorrect HBlank value under certain conditions
    • HTML and Text reports are not fully functional, add HDR and fix bugs
  • 0.97 - May 12, 2017
    • Fixed save issue in CEA Extended module, would not save correctly
4 people found this helpful

Outcomes