FAQ: Where can I find more information on the ADSP-BF609 EZ-KIT Lite/EZ-Board

Document created by CraigG on Mar 26, 2012Last modified by CraigG on Aug 28, 2013
Version 6Show Document
  • View in full screen mode

About the ADSP-BF609 EZ-KIT Lite

The ADSP-BF609 EZ-Board is the evaluation hardware for the latest BF60x family of Blackfin Processors. 

 

The evaluation hardware is designed to be used in conjunction with the CrossCore® Embedded Studio development tools to test capabilities of the ADSP-BF60x Blackfin processors, and can be purchased in one of two packages:

  • ADZS-BF609-EZLITE– This package contains the BF609 EZ-Board, power supply, Stand Alone Debug Agent (SADA2), USB cable and 2GB Memory card.
  • ADZS-BF609-EZBRD – This package does not contain the Stand Alone Debug Agent (SADA2), and requires an Analog Devices USB-based Emulator or Debug Agent board.

 

 

For more information see the product page here.


 

 

Manual

The ADSP-BF609 EZ-KIT Lite Evaluation System Manual is available, together with our other Blackfin documentation, from the Blackfin Manuals page on our website.

 

 

Examples and Board Support Packages

CrossCore® Embedded Studio includes a number of examples for the ADSP-BF609 EZ-KIT Lite, covering the System Services, and Device Drivers for the on-chip peripherals.

 

 

Examples for the off-chip peripherals, including the Power-On Self Test (POST) and Device Programmer Interface Applications (DPIA) for parallel and serial flash, are available as part of the BF609 Board Support Package.

 

 

 

Licensing

CrossCore® Embedded Studio is a licensed product. To use the ADSP-BF609 EZ-KIT Lite, Board Support Package and CrossCore® Embedded Studio you will need to have a valid license. Licensing information is available here.

 

 

Support Links

Questions specific to the ADSP-BF609 EZ-KIT Lite, associated examples and Board Support Packages should be posted within the Hardware Tools community on the EngineerZone, here:

Hardware Tools

 

 

Questions specific to the ADSP-BF609 processor architecture, peripherals, programming, applications and hardware design, should be posted on the BF60x community on the EngineerZone, here:

ADSP-BF60x

 

 

Private support is available by submitting a support request here.

Attachments

    Outcomes