FAQ: What examples are included in the Board Support Packages and CrossCore® Embedded Studio?

Document created by CraigG on Mar 26, 2012Last modified by CraigG on Aug 28, 2013
Version 5Show Document
  • View in full screen mode

Question:

I have recently installed CrossCore® Embedded Studio. Where can I find examples within the installation?


 

==========================

Answer:

The Board Support Package for your evaluation hardware is available to download from the relevant product page. This package provides all the necessary components needed to use your EZ-Board or EZ-Extender with the CrossCore® Embedded Studio software development tools.


 

There are two categories of HW controllers: On-chip and off-chip. On-chip controllers are defined as controllers that exist in the processor silicon package. Off-chip controllers are defined as controllers that do not exist in the processor silicon package but have been added to the EZ-Board or EZ-Extender.


 

Once you have installed a Board Support Package, it will allow you to connect to your new target board and access additional examples and SSL 2.0 drivers for off-chip controllers, and documentation for the EZ-Board or EZ-Extender.


 

By default, the location of any Board Support Packages you install can be found at “C:\Analog Devices\”, with examples located in a “.\<Your EZ-Board Software Version>\<Your EZ-Board Name>\Examples” directory.


 

All on-chip controller drivers are delivered as part of the CrossCore® Embedded Studio distribution. You can find example projects in the following directory:

<Install Dir>\CrossCore Embedded Studio 1.0.0\Blackfin\Examples

Attachments

    Outcomes