FAQ: Can we connect EI3 SDP Breakout Board and New DSP EZ-KITs ?

Document created by Reva@14 Employee on Aug 10, 2018
Version 1Show Document
  • View in full screen mode

Question:

 

Can we connect EI3 SDP Breakout Board and New DSP EZ-KITs?

 

Yes, We can connect the below boards:

 

ADSP-BF707 EZ-KIT Lite

ADSP-SC589 EZ-KIT Lite

ADSP-SC584 EZ-KIT Lite

 

The System Demonstration Platform Breakout Board provides a means to monitor each of the SDP’s 120 pin connector’s signals individually. Each of the 120 signals on the connector interface is exposed on the breakout board using through-hole probe points.

 

The SDP Breakout Board has a 120 pin receptacle connector for connecting to the SDP boards 120 pin header. It also has a 120 pin header connector to allow a daughter board designed for the SDP to be connected onto the Breakout Board. In this way, the Breakout Board can simultaneously connect to an SDP and a daughter board allowing the user to monitor the signals traveling between the two boards.

 

The SDP breakout board contains 240 through-hole probe points, 2 × 120 pin receptacle connector and 2 × 120 pin header connectors. One of the 120-pin receptacle connectors (J1)can be used to connect to the 120-pin connector on the SDP controller board. One of the 120-pin header connectors (P1), on the back of the SDP board, can be used to connect to a daughterboard (P1).

 

Connector J2 and P2 are for use with future Blackfin® EZ-Kit products.

 

For more details, please take a look into the chapter 'Through-hole probe points' in the below link:

http://www.analog.com/media/en/technical-documentation/user-guides/UG-282.pdf

https://wiki.analog.com/resources/eval/sdp/breakout_board

http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/sdp-breakout-board.html#eb-overview

 

 

 

This document was generated from the following discussion: Can we connect EI3 SDP Breakout Board and New DSP EZ-KITs?

Attachments

    Outcomes