FAQ: How to generate a makefile from a VisualDSP++ project?

Document created by Reva@14 Employee on Aug 10, 2018
Version 1Show Document
  • View in full screen mode

Question:

 

How to generate a makefile from a VisualDSP++ project?

 

Answer:

 

There is no command line switch to generate a makefile from a VisualDSP++ project. However, there are ways this can be achieved through the VisualDSP++ Automation Interface.  The makefile generation is done through the ADspProject object's "ExportToMakefile" method, export the makefile using a script.

 

For more information, see the documentation at 'Help: Contents: Automation: Automation: API Reference: ADspProject:ExportToMakefile'.

 

 

This document was generated from the following discussion: Command line VDSP - export makefile

Attachments

    Outcomes