FAQ: How to find the size of program in CCES?

Document created by Reva@14 Employee on Jul 20, 2018
Version 1Show Document
  • View in full screen mode

Question: 

 

How to find the size of the program in CCES?

 

 

Answer:

 

The map file describes how objects and the symbols they define are mapped into the memory defined by the .ld file.

 

We can type the following command in the additional options in the linker settings (Properties > C\C++ Build > Settings > Tool Settings > CrossCore GCC ARM Embedded linker > Additional Options). This will generate a map file for you in the debug folder.
 
-Wl,-M=ARMcode.map

 

Also refer in the below thread for more information:
https://ez.analog.com/message/247717

 

 

 

This document was generated from the following discussion: Find Cross

Attachments

    Outcomes