FAQ: Difference between ADIS1700x Demo and ADVS200x Demo

Document created by NagarjunaG Employee on Oct 31, 2017
Version 1Show Document
  • View in full screen mode
  • ADIS1700x Demo: PC suite to demonstrate the capability of ADVS200x image capture and accelerometer readings from ADIS1700x platform.
  • ADVS200x Demo: PC Suite to demonstrate the capability of ADVS200x camera, particularly the high dynamic range, good contrast and motion detection via ADIS1700x platform.

 

Please note, the ADIS17001 evaluation demonstration packages are available as free downloadable packages from www.analog.com/adis1700. The following are the 2 packages:

  1. EDK: SnapSensor Library Evaluation Demo Kit Software (Rev 1.0.0)
  2. DEV: SnapSensor Library Development Demo Kit Software (Rev 1.0.0)

 

The EDK allows user to evaluate the ADIS1700x vision sensing camera module, and the DEV package allows user to evaluate the ADIS1700x vision sensing camera module and enables the developers to understand and build their own applications, Sample console applications, and other application codes as examples (supplied as reference with the development package).The development package gives additional flexibility to the user to build sample applications, change the ADVS200x parameters, including R/W them in to a file etc. For more information, please refer to the user guides supplied with the packages.

 

This document was generated from the following discussion: Difference between ADIS1700x Demo and ADVS200x Demo

Attachments

    Outcomes