AD7616-P FAQ - What are the differences between the AD7616 and AD7616-P?

Document created by AFrost Employee on Jun 9, 2017
Version 1Show Document
  • View in full screen mode

The AD7616 and AD7616-P have similar functionality, with a few key differences.

  • The AD7616 has both serial and parallel digital interfaces
  • The AD7616-P has a parallel only digital interface
  • The AD7616-P has relaxed timing requirements on read & write setup and hold times
  • In hardware control mode, more features are unlocked when using the serial interface (AD7616 only). In parallel interface mode (AD7616 and AD7616-P), some dual function control pins are used by the digital interface so may not be used for hardware control.
1 person found this helpful

Attachments

    Outcomes