ADIS16209 Datasheet Error: Address code length

Document created by NevadaMark Employee on Feb 6, 2017Last modified by NevadaMark Employee on Feb 6, 2017
Version 2Show Document
  • View in full screen mode
TITLEADIS16209 Datasheet Error: Address code length
DOCUMENT

ADIS16209 Datasheet

REVISIONE
LOCATIONPage 12 (click here), left column, first paragraph, line 8
DESCRIPTION

This references lists the address code length as 6-bits.  It is actually 7-bits. This only matters if you are trying read the PROD_ID register.

SOLUTION

The next revision of this datasheet will replace the "6" (yellow highlight) with a "7."  Until then, please be assured that this bit is active and that you can read the PROD_ID register, using DIN = 0x4A00 to request the contents of this register (which will flow out on DOUT, during the following 16-bit SPI sequence).

Attachments

    Outcomes