ADIS16209 Datasheet Error; SPI Address Code Missing MSB

Document created by NevadaMark Employee on Feb 6, 2017
Version 1Show Document
  • View in full screen mode
TITLEADIS16209 Datasheet Error; SPI Address Code Missing MSB
DOCUMENT

ADIS16209 Datasheet

REVISIONE
LOCATIONPage 6 (PDF): Figure 3, Figure 4
DESCRIPTION

The address code in the SPI protocol is missing its most significant bit.

SOLUTION

The next revision of this datasheet will insert "A6" into the two areas of yellow highlight.  Until then, please be assured that this bit is active and that you can read the PROD_ID register, using DIN = 0x4A00 to request the contents of this register (which will flow out on DOUT, during the following 16-bit SPI sequence).

Attachments

    Outcomes