What does "Tactical Grade" mean for a MEMS IMU?

Document created by NevadaMark Employee on Oct 14, 2016Last modified by NevadaMark Employee on Oct 19, 2016
Version 6Show Document
  • View in full screen mode

So what qualifies an Inertial Measurement Unit (IMU) as "Tactical Grade?"  The qualifying metric for IMU grading is the In Run Bias Stability (IRBS) in their gyroscopes, which represents its stability during benign conditions, which include the following: ideal integration (averaging) time, stable temperature, no inertial motion.  Yole Development classifies IMUs as "Tactical Grade" when their gyroscope's IRBS is in between 0.5 deg/hour and 5 deg/hour.

 

IEEE-STD-952-1997 (Appendix B) provides an industry-standard definition of IRBS, which defines it as the minima on the Allan Variance curve.  The following graphic identifies the Allan Variance representation of a population of ADIS16490 IMUs. In this case, the parameter is defined as the sum of the mean and one standard deviation, which means that 67% of ADIS16490 units will perform at this level, or better.

REFERENCES:

  1. ADIS16490 Product Page: http://www.analog.com/ADIS16490
  2. High-End Gyroscopes, Accelerometers and IMUs for Defense, Aerospace & Industrial, Yole Development, 2015
    1. NOTE: At the time of this post, Yole Development offered this insight in a free sample of their their report.  Click on the following link to check this out, or search "yole mems imu" to see their latest work on this topic:
      http://www.yole.fr/iso_upload/Samples/Yole_High_End_Gyro_January_2015_Sample.pdf

 

Was this helpful?  Like this page to track future comments and follow NevadaMark to receive notifications for more information on this topic, which will include a more in-depth discussion on applying the Allan Variance method to characterize the ADIS16490's gyroscopes and accelerometers.

Attachments

    Outcomes