ADV7480 Design Support Files

Document created by XavE Employee on Jul 28, 2016
Version 1Show Document
  • View in full screen mode

Attached and linked are several files supporting the development of systems using the ADV7480.


You can download zipped file collections.


We  recommend that if you download and use these documents, you subscribe  to email notifications for either the entire forum or at least this FAQ  by clicking on the menu to the right.  In this way, you will be  automatically notified if there are any comments or changes to this FAQ  or attached documents.  If the menu choice is "Stop email   notifications," then you are already subscribed.


ADV7480 Product PageLink to Product Information Web Page
ADV7480 DatasheetLink to Product Shortform Datasheet
UG-747Link to UG-747 (ADV7481 Register Control Manual). The ADV7480 is a derivative of the ADV7481. The register controls in this document therefore apply to the ADV7480, except for the controls related to the Analog Inputs and SDP, and the controls related to MIPI CSI TxB.
ADV748x_HardwareManual_RevPrB_2014-07-11.pdf   ADV7480/ADV7481/ADV7482 Hardware Manual
ADV748x_Recommended_Settings_PrA_2014-08-20.pdf   ADV7480/ADV7481/ADV7482 Recommended Settings Document    ZIP file of the document above
ADV748x_Eval_Board_UG_RevPrB-26-09-2013.pdfEVAL-ADV748XEBZ Rev. B Evaluation Board User Guide
adv748xebz-05-07-13_b.zipEVAL-ADV748XEBZ Rev. B Evaluation Board Files
adv748xebz-assy_b1.pdfEVAL-ADV748XEBZ Rev. B Evaluation Board Assembly
adv748xebz-mfg_b3.xlsxEVAL-ADV748XEBZ Rev. B Evaluation Board BOM
adv748xebz-pcb_b1.pdfEVAL-ADV748XEBZ Rev. B Evaluation Board Layout
adv748xebz-sch_b2.pdfEVAL-ADV748XEBZ Rev. B Evaluation Board Schematic    ZIP file of the four documents above
ADV7480 Required SettingsThese are the required I2C writes for the ADV7481. The ADV7480 is a derivative of the ADV7481. These scripts therefore apply to the ADV7480, except for the Analog input CVBS scripts, the Analog input YC scripts, the Analog input YPbPr scripts, the Analog Input Fast Switch CVBS scripts, script 08-15 and script 08-16. An application requiring MHL must use the software driver.
1 person found this helpful