Matchstiq SDR Platform

File uploaded by Lorin on Jul 19, 2016Last modified by lallison on Aug 8, 2017
Version 5Show Document
  • View in full screen mode
Epiq Solutions’ Matchstiq™ S10, S11 & S12 define the state-of-the-art in small form factor software defined radio platforms. Building on the success of the award-winning Matchstiq™ S1 and Z1 platforms, Matchstiq™ S10 provides increased RF flexibility, RF performance, and signal processing capacity, in a smaller and lighter package. The S11 adds the option to use the RF inputs as 2 phase coherent RX inputs. And the S12 extends the lower frequency range down below 1 MHz. Click at the bottom of this document to download the complete flyer.

Outcomes