How is GP Timer in SC57x/2157x different from that of SC58x?

Document created by nithya.koch Employee on Jun 10, 2016Last modified by lallison on Jun 10, 2016
Version 3Show Document
  • View in full screen mode

GP Timer in SC57x is same as that of SC58x with the addition of some new features, which are mentioned below:


1. Timer in SC57x has two new configurations namely, "Slave Trigger toggle" and "Ordered Slave Trigger toggle", to configure the trigger slave response.


2. The Timer Signal Routing , that is, the signals that are internally connected to the timer are different.


Please refer to the "ADSP-SC57x SHARC Processor Hardware Reference" for more details.