Programming PLL on ADSP-214xx processors

Document created by Mitesh Employee on May 9, 2016
Version 1Show Document
  • View in full screen mode

While programming PLL on ADSP-214xx processors, it is must that the user take care of using the workaround of the anomaly#15000020. For more details on the workaround, please refer to the corresponding anomaly sheet. For example, ADSP-2146x anomaly sheet is available at the link below:

 

http://www.analog.com/media/en/dsp-documentation/integrated-circuit-anomalies/ADSP-21467_21469-SHARC-Anomaly.pdf

 

To generate the correct PLL programming code automatically with VisualDSP++, one can as well use the plugin "Expert Code generator" provided with the application note EE-322. It is available at the link below:

 

http://www.analog.com/media/en/technical-documentation/application-notes/EE-322rev5.pdf

1 person found this helpful

Attachments

    Outcomes