FAQ: DPM - Different wake-up sources on ADSP-CM41x

Document created by leonahi Employee on May 2, 2016
Version 1Show Document
  • View in full screen mode

Following are the wake-up sources on ADSP-CM41x from deep-sleep.

  1. Wake0 : PC05 - General purpose wake-up source
  2. Wake1 : PD00 - General purpose wake-up source
  3. Wake2 : PF08 - General purpose wake-up source
  4. Wake3 : PA11 - General purpose wake-up source
  5. Wake4 : JTAG - Wake-up through JTAG

 

Bit 0 in *pREG_DPM0_WAKE_EN corresponds to Wake0

Bit 1 in *pREG_DPM0_WAKE_EN corresponds to Wake1

Bit 2 in *pREG_DPM0_WAKE_EN corresponds to Wake2

Bit 3 in *pREG_DPM0_WAKE_EN corresponds to Wake3

Bit 4 in *pREG_DPM0_WAKE_EN corresponds to Wake4

Attachments

    Outcomes