FAQ: What is Logic Block Array? How is it useful?

Document created by SachinV Employee on Apr 29, 2016
Version 1Show Document
  • View in full screen mode

      Logic Block Array (LBA for short) consists of several Logical Blocks which can be programmed to perform logical or arithmetical operations. LBA module can output a logical state on its pin using a look table for its input combination ( Look up table mode) or It can be also programmed  as an AND-OR Array and generate product terms.   

    As this module can be used to generate the variety of logical functions, it obviates the need of small FPGAs in the system design.

Attachments

    Outcomes