How can I boot an ADSP-21584 based SHARC application?

Document created by Mitesh Employee on Apr 26, 2016Last modified by Mitesh Employee on Dec 9, 2016
Version 2Show Document
  • View in full screen mode

By default, CCES provides the ARM based init code. For booting ADSP-21584 based SHARC applications, SHARC init code may be required. Attaching an example init code which can be modified as per the system requirements (CGU/DMC settings). Make sure that the following steps are taken care while generating the loader file:


1. Select the SHARC init code executable as shown in the following screenshot.


2. Select the ADSP-21584 dxes as shown in the below screenshot.

1 person found this helpful