ADIS16460 Data Ready During Start-up

Document created by NevadaMark Employee on Apr 2, 2016
Version 1Show Document
  • View in full screen mode

The ADIS16460's data ready signal provides a pulse, every time that new data loads into its output data registers.  By changing states while the actual register update is happening, the data-ready provides an effective indicator for the "do not read time."  Therefore, triggering on the second edge of the pulse assures avoidance of data collision and minimizes latency.  During start-up, while the internal processor is initializing itself for sensor data sampling and processing, the data-ready will go through two non-operational states: an intermediate level, followed by a zero level.  After the initialization process completes, the data-ready signal will start pulsing once data production begins.  The following picture illustrates this process, where normal pulsing starts ~265ms after application of +3.3V on VDD.

 

EZ_FAQ_ADIS16460_DataReadyAtStartUp_00.png

 

The following picture provides a zoomed view of the time that the data ready stars pulsing, when the ADIS16460's configuration uses the internal sample clock and no decimation (nominal = 2048SPS). 

 

EZ_FAQ_ADIS16460_DataReadyAtStartUp_01.png

Attachments

    Outcomes