Next Generation ADIS16305?

Document created by NevadaMark Employee on Mar 27, 2016
Version 1Show Document
  • View in full screen mode

Q:

I just noticed that the ADIS16305 is not recommended for new designs.  What can I use in its place?

 

A:

The ADIS16305 provide a 4DOF (degrees of freedom) function, which has 1-axis of gyroscope sensing and 3-axes of accelerometer sensing.  Since there are no other 4DOF functions in this product family, a 6DOF product (3-axis gyro/3-axis accelerometer) would be the most applicable function to look for.  Here are two options to consider:

  • The ADIS16365 provides the same performance and function as the ADIS16305, but would present some size and cost trade-offs.
  • The ADIS16460 is closer to the ADIS16305, in terms of size and cost, but its gyroscopes have lower dynamic range (+100deg/sec).
  • The ADIS16445 and ADIS16448 are also worth consideration as well.

Attachments

    Outcomes