Kernel panic when booting from SD card

Document created by Aaronwu Employee on Mar 16, 2016Last modified by lallison on Jun 13, 2016
Version 2Show Document
  • View in full screen mode

Question:

 

I'm following the official quick start guide to boot from the SD card, it works fine with the prebuilt kernel vmImage file released in the CCES Linux Add-in package, but when I try to use my own built kernel vmImage, I get error kernel panic message like following, what should I do?

 

Kernel panic - not syncing: junk in compressed archive

CPU: 0 PID: 1 Comm: swapper Not tainted 4.0.0-ADI-1.0.0 #6

Hardware name: SC58x-EZKIT (Device Tree Support)

[<c00138b4>] (unwind_backtrace) from [<c001106c>] (show_stack+0x10/0x14)

[<c001106c>] (show_stack) from [<c034efec>] (panic+0x90/0x1e4)

[<c034efec>] (panic) from [<c04ce090>] (populate_rootfs+0x30/0xb8)

[<c04ce090>] (populate_rootfs) from [<c000881c>] (do_one_initcall+0x8c/0x1d8)

[<c000881c>] (do_one_initcall) from [<c04ccd9c>] (kernel_init_freeable+0x144/0x1e4)

[<c04ccd9c>] (kernel_init_freeable) from [<c034ddb4>] (kernel_init+0xc/0xe8)

[<c034ddb4>] (kernel_init) from [<c000e1a0>] (ret_from_fork+0x14/0x34)

---[ end Kernel panic - not syncing: junk in compressed archive

random: nonblocking pool is initialized

 

Answer:

 

The default buildroot configuration is for using with the RAM boot uImage, when build vmImage for SD boot, try to disable the following item in buildroot menuconfig:

 

 

make menuconfig:

filesystem images->

[ ] initial RAM filesystem linked into linux kernel

2 people found this helpful

Attachments

    Outcomes