Downloading evaluation software for AD7763 Evaluation Board from CD

Document created by MClifford Employee on Mar 9, 2016
Version 1Show Document
  • View in full screen mode

When downloading the evaluation software for AD7763 from the CD you may come across the following error showing when the install is ~25% through the completion bar.


This error is a remnant of the transfer of the installer from CD ROM to your PC.

Running the same installer downloaded from a USB stick, or downloaded from the AD7763 evaluation board page will not show up.

this proves that the error is related to the CD ROM transfer.


Advice here is to click on "Ignore".

Continue the install.

On completion of the install there is no effect on the operation of the evaluation kit and the software runs correctly.