SFP-RDK : ROSA, TOSA LED - source & schematic of SFP-RDK

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

Can I get source & schematic of SFP-RDK?

 

Yes, please see attached the schematic for one of SFP module reference designs.
Please note, the ADN2870 can be replaced with ADN2872 to get better performance.

The SFP-RDK includes:
- SFP Transceiver Module Board
- SFP Host Board
- JTAG Adapter board
- PCB Schematics
- PCB Layout , Gerber Files, CAD Files
- Bill of Materials
- SFP Firmware Source Code in ANSI C
- Evaluation GUI software
- Applications Note(AN-706), User Manuals

The SFP-RDK consists of Analog Devices’ optical
transceiver chip set: the ADN2870 dual loop laser driver,
the ADN2880/2 Transimpedance amplifier, the
ADN2891/2 Limiting amplifier and the ADuC7020
MicroConverter®. Use of the micro-controller allows
flexible module designs support user definable functions.
Figure 1.
1 person found this helpful

Attachments

Outcomes