Replacement for PMI119-883

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I am looking for a replacement for comparator PMI119/883 and  was wondering if
you still
produce the above comparator or have a direct replacement?

 

Here is the obsolete report on PM119Y/883C:

Obsolete Part Data

Generic Number: PM119
Description: Comparator, Dual
Obsolete Part: PM119Y/883C
Replacement: AD790
Is replacement pin compatible? No, part is a functional equivalent, not pin for
pin
 
Replacement Manufacture: This Model and all models in the family are obsolete
Last Order Date: 9/30/1996
Last Delivery Date: 3/31/1997

The recommended replacement is AD790. This is a functionally equivalent device,
it is not a pin for pin replacement.

If you need the wide operating temperature range, the part number AD790SQ has a
military operating temperature of −55°C to +125°C and comes in an 8 lead CERDIP
package.

The datasheet can be found on our website at:   www.analog.com/AD790

Attachments

    Outcomes