OP284F

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

The OP284F data sheet says that the storage temperature is between -65ºC  to
150ºC and operating temperature is between -40ºC to 125ºC. I am wondering if
OP284F will work with reduced performance at -55ºC?

 

Please be aware that the ADA4084-2 is a recommended replacement for the OP284.

www.analog.com/OP284

Newer Alternatives: NEW DESIGNS consider the next generation ADA4084-2 with
twice the bandwidth at half the power consumption in smaller packages.


The OP284 Absolute Maximum Rating for operating temperature is -40°C to 125°C.
It is not recommended to use the part at temperatures below -40°C because the
part is no longer supported by Analog Devices and not gauranteed for use. This
goes for any of the Absolute Maximum Ratings.

Attachments

    Outcomes