OP184: Replacement with the AD820 and NULL Pin

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is it possible to replace the op AD820  with the op OP184? What means the pin
connection NULL?

 

The OP184 and AD820 share a similar pin out but they vary significantly in
their bandwidth, offset, and noise. I would not consider them to be drop in
replacements. The decision will be made based on the specific applications. You
need to analyse your circuit requirements and determine whether the OP184 and
AD820 can meet these requirements.

The Null function on the AD820  is used to trim the input offset voltage. It is
an optional function (only available on the DIP package) which is described in
figure 19 of the REV.C datasheet.

A 20K resistor between pins 1 and 5 with the wiper to the negative terminal.
The null range is +-1mV which is good for this part.

Attachments

    Outcomes