OP1177/OP2177/OP4177 addtional information on slew rate 

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I'm looking for information about slew rate of the OP2177.

In the datasheet there is only a typical value with one load  (0.7V/µs).

Do you have more data:
- Min / max value over the temperature  range
- variation with the load

 

The slew rate is determined primarily by the tail current and the comp cap.
Taking into account process and temperature, We would say -30% to +20%.

For load, obiviously if you put 1,000 microfarads on the output, it will barely
move. Depends on the load and when the output stage goes into current limit.
(Which varies with temperature also).

Attachments

    Outcomes