HMC_T2220: RS232 interface pin out and communication set up

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I have signal generator HMC-T2220 and would like  information on pin out of
RS-232 interface and its transmission
characteristics. 

 

Please see below the pinout for the RS232 interface. It is a standard RS232
interface.

Here is the pin-out.



RS232_RXD0:     INPUT
RS232_TXD0:      OUTPUT

Baud:                    115200
Data:                     8-Bits
Stop Bits:             1
Parity:                   None

Communication is same as all other command interfaces.


Attachments

    Outcomes