EVAL-AD7719-EBZ Evaluation Board

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I want to know if the EVAL-AD7719-EBZ Includes cable with connector for 36 pin
connector and 9 pin connector


Please be advised that there are no cables included with this evaluation board.
The software that comes with this board is designed to work on Windows XP or
earlier, extra steps may be required to get this software to run on newer
versions of Windows. The software which ships with this board only works
through the parallel port (36 pin connector). The additional serial port (9 pin
connector) is included to allow the customer to interface to another system or
board using their own software.