ADXRS61x range change similar to ADXRS300

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

wants to expand the measurement range from 300°/s to 1200°/s. With the ADXRS300
it is possible by changing the value of an external resistor, can this
technique also be used with ADXRS610?

 

The functional blocks of both devices are similar and the technique referred to
in the ADXRS300 datasheet and in application note AN-625 for increasing the
measurement range is also valid for the ADXRS61x.

Attachments

    Outcomes