ADXL362 Self Test Procedure

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

I'm trying to use the Selftest feature: I've set Range to 2g, output is 100Hz.
I read the X-Y-Z before the Seltest command and after, the values don.t change
at all.  When I read Selftest register (0x2E), it returns 0 instead of 1 (ST
bit is asserted).
I've followed the Selftest procedure in the Manual page 41, "Using Self Test".

 

Please follow the process in this attachment to do the selftest for ADXL362.

Attachments

Outcomes