ADXL362 register configuration

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 3Show Document
  • View in full screen mode

We want to use the trigger function to store the pre & post instants of the
trigger event, to analyze the signal. The register configuration is attached.
Fifo reading is done after buffer complete, 500 ms after the interrupt. Our
intention is to read 50 ms before event and rest after the event till complete
the buffer. Could you help with the right register configuration ??

 

You can try the corrected configuration (attached) based on your intention
("Our intention is to read 50 ms before event and rest after the event till
complete the buffer.")

Attachments

Outcomes