ADXL78 temperature coefficient

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Our customer used ADXL150, ADXL105, ADXL190, ADXL250 and ADXL278 before, and
she found the relation between the output and temperature is monotonic. That
is: if the temperature increase, the output will increase too. Now she used
ADXL78, and she found the relation isn't monotonic. Below is the output of
ADXL78 at -40 degree, 10 degree and 60 degree. Whether the ADXL78 is
non-monotonic with temperature? Whether we have single-axis product which
output is monotonic with the temperature? Thanks!

                            -40 degree    10 degree     50 degree
Chip1 Output        653mV          738mV          634mV
Chip2 Output        671mV          735mV          680mV
Chip3 Output        635mV          712mV          687mV    

 

I have discussed the issue of a “monotonic temperature response” with the
designers, and it seems well known that the XL78 family is not monotonic with
temperature.  This is consistent with what the customer had reported.

Analog also offers the XL180, XL950 the XL001 for single axis acceleration
sensing.  Based on the characterization data for the XL950 and XL180, it would
appear that the behavior of those devices is monotonic.  However, please keep
in mind that this behavior is NOT guaranteed by Analog, and there is always the
possibility that a device will not have a monotonic temperature response.  We
do not currently have characterization data for the XL001, however if the
customer is curious about this device (it is a new, not yet released,
industrial vibration sensor) then I can report back once we have collected some
data.

Attachments

    Outcomes