ADXL345 internal filter

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Could you give us some more detail of the ADXL345 insite

 

The internal filter is as follows:
1. There is a single pole analog anti-aliasing filter at ~1.6kHz.
2. The digital filter is an IIR type, first order.
3. The mechanical system acts as a two pole filter above ~7kHz.

As far as design particulars of the filters are concerned – that’s proprietary
information that we do not share.

Attachments

    Outcomes