ADXL213: Magnetic field area

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can the Accelerometer ADXL213 work in a magnetic field area?

 

The sensor in the accelerometer is a polysilicon surface-micromachined
structure built on top of a silicon wafer. The operation of the accelerometer
is unaffected by magnetic fields.

Note that the ADXL213 LCC package has a metal lid and should not be used in
strong magnetic field applications such as MRI scan. In such a case I would
recommend the ADXL322

Attachments

    Outcomes