ADVFC32_input range

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

When configuring ADVFC32 as Positve Input Voltage V/F Conversion(Figure 1 in
the datasheet), what range of the VIN? I think it can't exceed 15V, isn't it?


The maximum input range is 0-10V. Smaller input ranges such as 0-1V can be used
but 0-10V is the maximum range.