ADV7393: Output tri-synce at 3G data rates?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I am looking at using the ADV7393 to output tri-sync, can this do this
at 3G data rates (clock = 148MHz) to lock a picture resolution of
1920x1080p (60Hz)

 

I got the following from our Product Line:

No, I’m afraid the ADV7393 (or any of the encoders) cannot support 1080P at
60Hz. They cannot handle the 148MHz input clock frequency.

Attachments

    Outcomes