ADuM5401: Is 1 Mbps the maximum data rate, can this device be used above 1 Mbps?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

For the ADum5401ARWZ a Maximum Data Rate of 1 Mbps is given. Is this data rate
a useful operating rate or is
this the absolute maximum rate? what will happen to the signal above 1 Mbps?


1 Mbps is the maximum data rate for the A grade ADuM5401 part ADuM5401ARWZ. If
your data rate may exceed 1 Mbps then I recommend that you use the C grade
part, ADuM5401CRWZ which has a maximum data rate of 25 Mbps.