ADUM54xx: Can I make parallel connection of devices in a redundancy configuration?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can I use the ADUM54xx devices in a redundant parallel configuration? I would
like to use two ADUM54xx in parallel so that I could have some redundancy in
case of failure? What are the issues in this type of parallel connection?

 

It is a little tricky to use these parts in a redundant parallel
configuration.  The main issues are:

1) the power supply sections should be diode ORed so that if the fault is on
the Viso side, it can not drag both units down.  This also prevents the units
from back driving each other.

2) the data outputs can not simply be connected together.  Assuming one device
is "on" and one is "off".  A high output on the active device would be
connected to an inactive output on the device that is off.  This will power
the isolated side of the "off" device through the ESD protection diodes.  Once
the secondary side of the "off" device comes up, its outputs will default to
low.  But this output is already being pulled high by the output of the "on"
device  This will cause large currents to flow, probably 30mA on the output
and an additional 90mA on the VDD1 line, and the output will go to an
undetermined state.  Probably half of Viso.

The solution is again to diode OR the outputs together with pull down
resistors to be sure it goes low when required.  The speed of the output will
depend on the size of the pull down resistor, the smaller the value, the
faster the output will slew low, but the more current the output will require.

Attachments

    Outcomes