Can ADUM3440 be used to provide Isolation from high frequency noise?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can these devices isolate (filters out) high frequency noise.


The ADuM3440 doesn’t explicitly filter high frequency noise, but it does block
current flow from one side to the other so noise is isolated. The typical
capacitance across the isolation barrier is 2.2 pF, so a small amount of nose
at 400 MHz might be seen.

We advise designer's to use extra filtering from traditional techniques to
boost the filtering performances.