ADUM4160/ADUM3160: Can these devices support OTG (On The Go) USB?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can ADUM4160 support OTG (On The Go) USB?

 

The ADuM4160 does not support On The Go. This part of the USB specification has
modes where power is not present on the cable, and we can not pass signals to
initiate communication if power is not present. We recommend dedicated host and
peripheral ports if isolation is required.

Attachments

    Outcomes