ADuM3220: What is the practical use of the two Junction to Case thermal resistance values?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

There are two Junction to Case thermal resistances but what is the practical
use of these?

 

The junction to case thermal resistance can be used in applications where the
case temperature is known. There are two junction to case thermal resistance
values because the device contains two die, side 1 and side 2.

Attachments

    Outcomes