ADUM3070 Creepage and Air Clearance specifications

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What are the specification for creepage distance and air clearance for
ADUM3070? Datasheet states minimum spec; what are the actual values?


The creepage of the ADuM3070 QSOP package is on average 3.26mm, the average
line of sight clearance is about
4.3mm assuming good pin shape.