FAQ: Can we bundle SigmaStudio with our product design?

Document created by JeradL on Jul 13, 2010
Version 1Show Document
  • View in full screen mode

No, the SigmaStudio software is licensed for use as a design tool and is not intended for use as a mass-market tuning/programming tool. If your product design requires a software interface for tuning audio parameters, then you should develop one that fits your product's need. SigmaStudio includes too many features that are more than what a consumer will need to interface to the audio processor - there's too much of a chance for them to do something they they (and you!) don't want them to do.


SigmaStudio does include many features for easing the integration of a SigmaDSP into a product design. These include C header file generation, the Capture Window's detailed display of data being written to the SigmaDSP from SigmaStudio, and microcontroller-ready program and parameter data files.



This FAQ was generated from the following discussion: Can we bundle SigmaStudio with our product design?