ADUM4160/ADUM3160: What is the difference between these 2 USB isolation devices?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the difference between the 2 USB isolation devices, ADUM4160/ADUM3160

 

There are two differences, insulation rating and operating power supply range.

ADUM3160:  Insulation Rating : 2.5kV rms , power supply: 4.0 V to 5.5 V
operation
ADUM4160:  Insulation Rating : 5kV rms , power supply: 3.0 V to 5.5 V operation

Attachments

    Outcomes