ADuM2400: 12 V digital signal

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I'm interested in details about ADuM2400 icoupler input as i should handle 12V
digital signals.

 

The maximum supply voltage that can be used with thjs icoupler is 7Volts, and
the i/p's and o/p's must stay within 0.5Volts of the supplies, so therefore you
cannot use 12 volt digital signals with these devices.

Attachments

    Outcomes