What's the difference between the ADuM1440/41/42 and the ADuM1445/46/47?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What’s the difference between the ADuM1440/41/42 and the ADuM1445/46/47?

 

All devices in the family contain a refresh circuit to guarantee dc correctness
at power up. If no pulses are received on the secondary side of the transformer
for approximately 200 µs, the input side is assumed to be unpowered or
nonfunctional and all outputs are set to a default state. The ADuM1440/41/42
output default is high, while the ADuM1445/46/47 output default is low.
1 person found this helpful

Attachments

    Outcomes